Part Number: INA128
Hi,
Does anyone know how the settling time for INA128/129 was measured or spec'd? When filling out the datasheet, what was the output swinging from to arrive at a 9 us setting time? I only ask because I plan on swinging the output from the positive rail to ~3 V, so I was hoping to understand what the settling time might look like for a transition like that.
Also, a question about the input voltage ranges. The spec for input common mode voltage range (which I understand to be the average of the inverting and non-inverting inputs) has a max of 1.4 V lower than the positive rail, but the datasheet also says that the inputs are protected to +/- 40 V. My question then is what happens then if the input (V+ - V-) is at 40 V, which surpasses the spec for input common mode voltage? How will this affect the behavior of the amplifier?
Regards,
Michael