This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM339A: Can it be powered by +/- asymmetric power supply?

Genius 3900 points
Part Number: LM339A


Hi,

we use LM339A as comparator under +/- power supply. there are two situations we need to confirm. 

(1) V+ = +5.3V and V- = -5.3V

(2) V+ = +18.5V and V- = -5.3V

Coudl work noramlly under these power supply? If it can, what is the input voltage range and Vout High/Low range? 

As in datasheet, the efffective Vin is 0~VCC-2V.

Thanks!

  • Hi Yi,

    the recommended common mode input voltage range translates to

    (1) -5.3V...+3.3V

    (2) -5.3V...+16.5V

    in your application.

    Vout_low would also be -5.3V. Vout_high depends on the supply voltage of the pull-up resistor. The pull-up's supply voltage should be no higher than +30V - 5.3V = +24.7V.

    Kai