Part Number: THS7530
Other Parts Discussed in Thread: TINA-TI, , THS4541, OPA859
Tool/software: TINA-TI or Spice Models
Hi everyone,
This is a case where the THS7530 works but then it doesn't. It is just weird. I have attached the TINA TSC file for re-production of the issue.
If the analog chain includes the OPA859s, the THS7530 doesn't work. With the OPA859s or without them the VM1 & VM2 are exactly the same which means same CM and same differential swing.
Is there anything i should set-up in TINA. My version is the free 9.3.200.277 SF-TI.
This is the case with the SW1 & SW2 closed, SW3 connecting R5 with R4&R7 and SW4 connecting R6 with R7&R41
This is the case with the SW1 & SW2 open, SW3 connecting VG1 with R4&R7 and SW4 connecting VG1 with R7&R41
Am i missing anything here?
Regards
Manos