Other Parts Discussed in Thread: VCA8500
When I used default power up mode by VCA8500, I give it a 500khz 100mv AC signal,then the signal wasn't amplified,and present a square wave.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When I used default power up mode by VCA8500, I give it a 500khz 100mv AC signal,then the signal wasn't amplified,and present a square wave.
Hi,
Square wave occurs in cases when the signal chain gain is too high.
With 20dB fixed LNA gain, 20dB PGA gain, the signal chain gain is 40dB (assuming 0dB attenuation), this would amplify the signal amplitude by 100.
You may want to reduce the input amplitude and check.
in your plot, red plot shows about 250mVpp sine signal. make sure the Vcntl signal is applied correctly. 0V is min gain and 1.2V is the highest gain.
the setup has a lot of noise due to cables. we suggest you use SMA/BNC cable to minimize the coupling noise.
if you input 100mVpp, you can adjust the Vcntl to make the device out put unclampped waveforms. please note VCA8500 has clamp function on the VCA output as well. if signal is too big, the output will be clamped.
Thanks!