Dear Team,
May I know this IC's maximum power dissipation?
The engineer need to check the thermal performance,
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
May I know this IC's maximum power dissipation?
The engineer need to check the thermal performance,
BR
Kevin
Hello Kuan,
As long as the junction temperature does not exceed 150°C, then the device has not exceeded its absolute maximum rating.
Anyway to determine the maximum power INA230 can dissipate under normal operating conditions we can assume VS=3.3V and VIN+=VIN-=VCM_max = 30V. Total power = Vs*IQ +VCM*IB.
So for I2C SCL frequency < 10kHz and TA = 25°C,
Ps = 3.3V*320µA =1.056mW
PCM = 30V*20µA = 0.6mW
Ptotal = 1.656mW.
For I2C SCL frequency < 10kHz and TA = 125°C,
Ps = 3.3V*395µA = 1.3035mW
PCM = 30V*20µA = 0.6mW
Ptotal = 1.9035mW.
For I2C SCR frequency = 2MHz and 25°C,
Ps = 3.3V*480µA = 1.584mW
PCM = 0.6mW
Ptotal = 2.184mW
In order to determine IQ and IB, I used Figures 13, 14, 16, and 18 of the datasheet.
Hope this address the question.
Best,
Peter