Other Parts Discussed in Thread: TLV2302, , LM358, TSM102, TLV7021, TLV9051
Hi,
LM392M (SOIC-8) is rated to work from 0°C to 70 °C, I was wondering if there is an equivalent part with the following temperature rating -40 °C to 85 °C?
Thanks in advance.