This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA308EVM: Unable to connect to board via USB

Part Number: PGA308EVM
Other Parts Discussed in Thread: PGA308

The PGA308EVM board is unable to connect with any of the computers at our office. We have tried multiple boards, multiple computers, changed all the wires and power supplies, and even went as far as to order a new board to ensure that the others that we had hadn't degraded. The only screen that we get is the typical USB Communications problem popup that you get if you try to run the PGA308 cal software without the EVM board plugged in.

  • Hi Adam,

    Please verify the following:

    1) Can you please verify all jumpers on the PGA308EVM and the USB DAQ board are in the correct.  Specifically, Can you please verify/confirm on the USB DAQ board that  JUMP3 is in the EE_ON position as shown below? I have seen a couple of USB DAQs that are configured with the wrong jumper settings causing this issue.  Please see the image below, with the jumpers highlighted in red.

     2)  When installing the software, it is important to run the installer executable with administrator privileges. You could attempt to uninstall the software and reinstall as administrator.  To uninstall the software, navigate to Control Panel -> Uninstall or change program and right click on PGA309EVM-USB and click uninstall.  To re-install the software with administrator privileges, download the PGA309EVM-USB software from http://www.ti.com/lit/zip/sboc320 and save the file on your PC.  Unzip the sboc320 folder, and navigate to the setup.exe file.  Right click on the setup.exe and select Run as administrator.  Follow the prompts to complete the installation.

    If after setting up the jumpers, and re-installing the software with administrator privileges, the issue persists, please post a snap shot of the USB Communication problem popup you are getting.

    Thank you,

    Kind Regards,

    Luis

  • HI Adam,

    I have not heard from you, I am assuming this resolved the PGA308 EVM issue; however, please post if the USB communication issue persists.

    Thank you and Kind Regards,

    Luis