I am trying to simulate VCO circuit using OPA189 in TINA with no success Could you help in resolving the problemVCO_Test.TSC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to simulate VCO circuit using OPA189 in TINA with no success Could you help in resolving the problemVCO_Test.TSC
Hi Gary,
because the -input of OPAmp sits on virtual ground, T1 has no effect when being turned-on or turned-off. This circuit cannot work. Where do you have this circuit from?
Kai
Hi Gary,
Thank you for your post. Many of us are on holiday break, so we will support you shortly.
-Tamara
Hi Gary,
Enclosed is an example of VCO with OPA189. If you have questions, please let us know.
Regards,
Raymond
Hi Gary,
you can shift the bipolar input signal and by this convert it into an unipolar signal which is needed by the circuit.
Can you tell more about your application? Why is a bipolar control input voltage needed? What shall be the effect of a negative control input voltage?
Kai
ok, it was a curious question. BTW, when we increase the simulation time to 1s, I get convergence error in TINA. Could you resolve the problem.
Can you explain what they mean? And I am also interested to get the same frequency for -2V as well. Purpose is academic