Other Parts Discussed in Thread: TLV3701
Hi, team,
Customer requires for TLV3701-Q1 input block diagram.And they would like to double check if there is ESD diode at (IN+-)-VCC and (IN+-)-GND and protection diode between IN+and IN-?
Thanks.
Johnny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, team,
Customer requires for TLV3701-Q1 input block diagram.And they would like to double check if there is ESD diode at (IN+-)-VCC and (IN+-)-GND and protection diode between IN+and IN-?
Thanks.
Johnny
Hi Johnny,
The TLV3701-Q1 does have ESD diodes at IN+ and IN-, but I am working on finding a block diagram for the part. If it is ok with you, I will email you the block diagram externally.
Regards,
Jonny
Jonny,
Thanks for reply, but is there any protection diode between IN+ and IN-?
Thanks.
Jonnyh
Hi all,
when you compare the datasheet of TLV3701 with that of TLV3701-Q1 the datasheet of TLV3701-Q1 appears to be incomplete. Sections 8 to 12 are missing.
I don't think that there are protection diodes between the inputs, because the specified maximum differential input voltage is +/-20V.
And I think that there are only internal protection diodes from the inputs to the negative supply rail.
Kai
Thanks for your input Kai!
Johnny,
Will it be ok for me to respond back to you next week when the team is back from holiday break? I should have some actual documentation to confirm this by then.
Regards,
Jonny
Jonny,
It's okay in you can send me some detail information after holiday. Thanks.
Johnny
Johnny
There are no diodes between the inputs. That is more common on high speed amps to prevent the inputs from drifting too far apart for the sake of response time to fast input transients.
Chuck