This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC7221: Device soft start with delay between applying V+ and V-

Part Number: LMC7221
Other Parts Discussed in Thread: TL331, TLV1701

Team,

my customer wants to implement some kind of soft start where there is a delay between applying V+ voltage and V- voltage.
The delay between applying V+ and V- is 150msec.

  • Do you see any issue with this delay?

They want to supply the device with +15V and -15V. As I see it, the device can handly a max range of 16V (V+ minus V-)

  • Is my understanding of the datasheet correct?

Thanks!

  • Franziskus

    Having a delay between V+ and V- being applied is not a problem as long as none of the abs max conditions are violated.  One area of concern would be the voltages applied to the inputs.  The inputs always must not exceed the supply pins by more than 0.3V.

    Your second question relates to the abs max supply voltage which has a maximum of 16V.  That means that the difference between V+ and V- can never be greater than 16V.  If the customer wants to apply +15V to V+ and -15V to the V- pin, that will be a supply voltage of 30V and violates the abs max rating.  If those are the required supply voltages of the system, I suggest using devices such as the TL331 or TLV1701 which are also open-collector devices that can accept supply voltages as high as 36V.

    Chuck

  • Thank you Chuck!

  • Chuck,

    a quick follow-up question regarding the delay between applying V+ and V-:

    Is this statement in general valid?
    I have a couple other comparators and op amps that are part of the same discussion.

    Thanks!

  • I would make the same comment regardless.  You really just need to look at what is connected to the inputs to determine if the delay is a problem.

    Another good tip when there is a concern about turn on delay is to put a resistor in series with the inputs or use a device that has a fail safe input.  Many of our new comparators like TLV701x/2x/3x/4x have this feature integrated.  A good way to look for this is in the abs max table.  If the input pin voltage rating is related to a voltage value instead of VDD or VCC or V+, than a voltage can be applied to the inputs regardless of the supply. 

    Chuck

  • Hi Franziskus,

    this post might interest you:

    Kai

  • Thanks Kai

    Franziskus

    If you need anything else, please let us know.  Otherwise, we will consider this closed.

    Thanks

    Chuck

  • Thanks Chuck and thanks Kai!