Other Parts Discussed in Thread: LM8272
Hello-
We need help picking an op amp and drive circuit for driving a highly capaciitive load. Refer tothe attached circuit diagram.
The original plan was to use the LM8272 to replace the AMP01, but the absolute max voltage spec on LM8272 is (V+, V-) 27 Volts. That is a problem in this application.
Can you suggest a higher voltage part (+/- 18V) at least, i.e. surface mount, dual op amp, cap driver…………. similar to LM8272.
Thanks and Best Regards,
Tim Starr on behalf of Al Kumar