Part Number: INA381
Other Parts Discussed in Thread: INA181
Greetings - I have a need to sense a 12vdc 3w lamp circuit (non-automotive) to see if the lamp is on or off. Not that I think it's important but the lamp can be in a flashing state with a frequency measured in many seconds. It's an existing piece of hardware that sinks the voltage to ground via IC, not mechanical. The "monitoring" will be accomplished by a mcu GPIO @ 3.3v. Tapping into the existing wiring is my only option, preferably after the lamp, as there are 2 lamps sharing a common 12vdc wire. I realize this this is a stretch outside the realm of an INA381 intended application, just more a curiosity if it possible and if so, would the INA381 accomplish the task?
TIA,
-Terry