This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM293: How to explain the LM293B IOH High-level output current 1uA?While the LM293 Open-Drain output~

Part Number: LM293


Dear TI Partners:

                           How to explain the LM293B IOH High-level output current 1uA?While the LM293 Open-Drain output~

                           Tks

BR

Cheney_Sun

                          

  • Hello Cheney_Sun,

    This is a "leakage current" that can occur at higher temperatures.

    While you tend to think of the output device as a discrete transistor, it is actually one of many devices on a die - so there are some leakages within the die to V+.

    These leakages are always there, even when the output is "low", which normally swamps out the leakage. But this leakage can cause issues if you use unusually high value pull-up resistor values (>1M) at high temperatures, and could cause the output high voltage to vary from the expected pull-up voltage.

    In the majority of applications, you will never notice this current.