Other Parts Discussed in Thread: OPA2210
Hello,
I am using eight LMH6321 PowerSO 8 package devices to provide higher current output capabilities for eight op-amps which are used for transducer excitation (Wheatstone bridges etc); there are two devices used per transducer excitation channel. My PCB has 6 layers of 1oz copper of which three are used for heat spreading. Other layers are used for signals and have been flooded with copper where possible to increase the spreading copper area. The board area is approximately 7 square inches and thermal vias are used to connect each plane together.
Using a thermocouple I have measured the case temperature as well as I can to be approximately 81°C with an ambient of 25°C when dissipating 1W of power. Only one channel is on at a time but there are other components on the board that contribute to the heat within the PCB. What I need to know is the junction temperature of the LMH6321.
The datasheet for the LMH6321 provides values for theta(JA) when dissipating 0.75W of power with various PCB stacks and copper areas (Table 2). Choosing the best case of around 82°C/W and multiplying by the power dissipated then adding on the ambient temperature gives a theoretical junction temperature of 107°C. Working back for theta(JC) would give 26°C/W but I am not convinced this is a particularly accurate figure knowing that if I drop the power dissipation by half, I should get a junction temperature of 66°C yet I measure a case temperature of 70°C.
Reading SPRA953C I understand that given a psi(JT) value I can estimate the junction temperature to a reasonably accurate value using the thermocouple method.
Do you have a psi(JT) value for this device please?
If you have any tips on how I can get an accurate junction temperature value I'd be very interested.
Thanks,
Simon