This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL062: Wrong output for voltage follower

Part Number: TL062
Other Parts Discussed in Thread: LM35, , TLV9102

I have the circuit of the second half of the TL062CP as a voltage follower as follows: IN2-  (pin 6) connected to output pin 7 pin 4 ground pin 8 +12v  pin 5 (IN2+) connected to output (pin 2) of LM35. Output of LM35 is .274 volts ; output at pin 7 of TL02CP is 0.675 volts instead of 0.274 . This is true when nothing but a dvm  is connected to pin 7 of TL062CP (it output 2 ) . I have not cleaned the board. This same voltage appeared on the previous board I made and nothing else is connected to this circuit to cause this error.