Part Number: LMC6001
Other Parts Discussed in Thread: LMH6321, BUF634, OPA564, ALM2402F-Q1
I would like to use TI's LMC6001 is integrate a signal between 3 to 10 VDC, but with 22 micro-A. The problem is to use output from the LMC to drive a st of trip logic (equipment protection circuit) using 2N3904 devices (firing at 200 mA). The specification for the LMC would appear not to allow (?).
I am a ME ... last time I took a EE course was 100 years ago, worrying about rise/fall times at N-P interfaces !!! Help.
PS I have a schematic indicating the desired signal conditioning (LMC 6001), and the trip logic downstream.