Other Parts Discussed in Thread: LMC6462, OPA251, OPA2188, LMC6482
Hello team TI,
Need suggestion for the following:
The circuit outputs a DC current of 6.18nA when the input voltage VG1 is 1V.
What changes should I make into the circuit so as to get a AC (sine wave) at the output?
Approach is to use a opamp based oscillator at the input.
Can you please help me for the requirement?
Attaching the circuit for reference.
Also, the pspice model contains a Lib file. When I tried to import the same in LTspice, I get an error 'unable to open OPA.lib' Any potential solution for this?