Other Parts Discussed in Thread: INA260, , INA190, INA229-Q1, INA228-Q1
Hello Guys,
Good day.
Our customer is using INA260 in measuring the current, voltage and power using Adafruit on the link below using their sample code ina260_simpletest.py However he's sample current measurements are 112.50mA, 52.50mA, -1.25mA, 53.75mA. As you can see, it always end with .50, .75, .25 or .00mA.
He wanted to know if INA169 will be appropriate for this application and will have better resolution than the 0.25mA step size he is getting with INA260?
Thanks in advance!
Art