Other Parts Discussed in Thread: THS4631
Dear TI expert,
I now use +18.5V and -13V as the power supplies of THS3062 and THS4631.
Now, I wonder if I can use +23V and -8V as supplies of THS3062 and THS4631?
Best
Yatao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Yatao,
From the datasheet in the sections titled Absolute Maximum Ratings and Recommended Operating Condition:
THS4631
So, for both devices, you may use a dual power supply of +23V and -8V. But, these supplies (31V) are above the recommended power supply of 30V and are instead closer to the abs max rating of 33V. Thus, the specs listed within in the datasheet will not be guaranteed at those power supplies. If you would like to be within the recommended range, an option would be to use +22.5V and -7.5V instead.
Thank you,
Sima