This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Using 4x INA303 together with DRV8313 (basically the TI reference design) for current sensing a BLDC.
I need the INA's to be considerably smaller.
Please help propose a few alternatives with similar specs and feature-set.
ps. it's wired up per below. alerts and out goes to the mcu
Hello Dav01,
Thanks for considering to use Texas Instruments. We have two other current shunt monitors with comparators that are in smaller packages. However, they do have some key differences from the INA303. One device is the INA301, which only has an alert but no analog output pin. The other device is the INA381, which has a lower bandwidth. Both devices only have one comparator and the delay for their ALERTs are not tunable.