Part Number: AM4372 Other Parts Discussed in Thread: TPS65218 , TPS65218D0 , TPS65910 , TPS65217 , TPS650250 , TPS6521825 , TPS6521815 , AM5728
Hi TI Experts,
I am working on a design using AM437x or AM438x processor family.
Checking if you have…
Part Number: TDA4VH-Q1
I have a camera, serializer, and deserializer, and I'm trying to capture video on CSI-RX.
What order do I need to enable the devices in? What issues may appear if the order is incorrect?
Part Number: TIDA-050026-23881
One of the main challenges of designing a multi-port system is supporting all ports on a full load using a limited power supply. TI’s FirmPSE system-level firmware solution provides designers with various power supply…
Part Number: TDA4VH-Q1
By default, CPSW does not pass VID 0 (priority-tagged) frames as-is. The Linux driver strips or replaces VID 0 at both ingress and egress, making it impossible for the use-cases that require VID 0 with priority bits set on the…
Part Number: TMS320F28P650DK
Understanding Ethercat:
Introduction to Ethercat by Beckhoff : EtherCAT Introduction
ETG.2200 EtherCAT, EtherCAT P and Safety over EtherCAT Slave Implementation Guide
Section I - Technology
Register Description…
Part Number: AM62P Other Parts Discussed in Thread: SYSCONFIG
The AM62P MCU+ SDK only provides McASP examples for the wkup-r5fss0-0 core.
How do I port McASP to run on the mcu-r5fss0-0 core with DMA support on the AM62Px platform?
Part Number: MSPM0-SDK Other Parts Discussed in Thread: MSPM0C1104 , MSPM0G3507
Small-package MSPM0 devices often run into hardware UART count limitations due to pin constraints. When you need more serial interfaces than the on-chip UART modules can…