Hi,
In my application I need to measurement the load current from 300V/4A isolated power supply. For that purpose, I'm wanted to use the AMC1100 Fully-Differential Isolation Amplifier in a High-Side measurement configuration (with floating5V power supply, VCC1). Before I'm implementing the circuit in my custom board, I need you to answer the following questions (which probably related to the same subject):
- According to the datasheet, the maximum input voltage before clipping is 320mV. Assuming that I have a 50mΩ shunt resistor, the max load current allow, even the momentary at startup of the 300V power supply, is 320mV/50mΩ=6.4A. My question is that: what is the maximum VINP – VINN voltage before damaging the devise? How can I see that from the datasheet?
- Again, Assuming that I have a 50mΩ shunt resistor, since the common-mode operating range is from –0.16V to VDD1 (5V), the device will not damage up until the 5V/50mΩ=100A (VINP – VINN will be 5V) Am I right?
Thanks a lot,
Idan