Part Number: INA260
Hi,
I want to measure votage of -5V 2A,I see the datasheet says the "common mode" votage is -0.3~40V. So,can I connect -5V to the VIN- pin to measure current ? and connect -5V to the GND measure the -5V votage(but AGND and DGND both is GND )? or convert the -5V to 5V then measure the 5V votage? see figure. Is that ture? or can you recommend a chip that can be used? Thanks