Hello
I wonder the input impedance LM2902.
Now, Vin(+)/(-) = 0.45V, Vout = 4.7V, Vcc = 6.8V
LED is in front of FET drain.
Inverting input is 750 resistor, but non inverting input isn't.
I test this circuit inserting the inverting 1K resistor.
The result is Vin(+)/(-) = 0.46V, Vout = 4.7V.
when 100K resistor insert the circuit, the result is
Vin(+) = 0.48V, Vin(-) = 1V, Vout =5.8V
I have any question.
Is it need the input impedance matching or how to calculation input impedance?
in order words, I want to know that 750 resistor must be inserted in non inverting input.
Thank you
Mike.