Other Parts Discussed in Thread: THS4631, OPA656, THS4601, OPA659, OPA657
Hi,
I'm working on a new design where the THS4631 would make an ideal input front-end for a user-provided analog signal. Ideally, this would be AC coupled in using a 1 uF and a 1 Mohm resistor, giving a nice low 1s time constant. The circuit is a simple non-inverting Gain=2 configuration after the AC coupling stage. Power supplies are +/- 15 V.
The problem I see is that, when the input gets up around 1 MHz and >3 Vpp, a *BIG* dc bias current starts flowing out of the non-inverting input of the THS4631. For example, at 1 MHz and 3.75 Vpp input, I measure 1 microamp of bias current through the 1 Mohm resistor to ground. The effect seems to have a strong threshold for input amplitudes above ~ 3Vpp; below that the bias current is much closer to the spec sheet 100 pA.
Is this a known "feature" of the THS4631? It seems like some input protection diodes are lighting up. I've seen the same behavior on 2 parts, and it shows up in unity gain as well as G=+2 configuration. If I short out the 1uF AC coupling capacitor, then the offsets completely go away (my sig-gen is 50 ohms, and the microamp DC bias doesn't move it much).
Thanks in advance,
--Matt