Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Measurement of currents from 1nA to 1mA

Other Parts Discussed in Thread: LOG114, LOG104

Hi, I need to measure currents from 1nA to 1 mA, the current comes from collector of PNP transistor in base-comon configuration. I tried to use transimpedance amplifier to measure the current, but the problem is that after 1uA the output of amplifier shows saturation and it is not possible to measure the complete current range. I would like to know if you can recommend me an amplifier or one correct configuration to measuring with precision the current. Below I show the basic circuit used.