Other Parts Discussed in Thread: BUF634, LMH6723
Hello,
I would like to use two BUF634 in parallel configuration for audio application (headphone amplifier).
I read Application Bulletin "COMBINING AN AMPLIFIER WITH THE BUF634" (sboa065.pdf) and have a questions about connecting BW pins.
In Bulletin BUF634 use maximum frequency bandwidth (BW directly connected to V- rail).
I would like to decrease bandwidth (or have possibility to change bandwidth during testing)
My question is...
1) Should I use individual resistors for each BUF634? Or can I use only One Resistor for all BUF634 (all BW pins connected in parallel and connected with V- with single resistor)?
I think one resistor is better, because multiple resistors (with different value due to tolerance) will provide different currents for BUF634`s and all BUF`s will be in a different mode.
But I`m not sure if this correct.
2) What is a best current (resistor value) in term of signal quality?