Other Parts Discussed in Thread: LM324, INA333, INA331
Im using a LM 324 quad op amp to design an instrumentational amp. I would like a gain of 1000. For the Rgain value i am using 2000 ohm resistor and for the R value i am using 1M ohm resistor. When i connect the 5V power supply and the laod sensors i get an output of 2.6V constant, regardless of whether ipush down on the load cells or not.. I am wondering what I am doing wrong. The voltage output should change in correspondence with pushing down on the load cell?
I am using a SEN-10245 load cell.
The equation i am using for the gain is Av = (1 +2R/Rgain)
I am trying to build a digital scale.
I loaded the circuit diagrams i am following
Any help on the subject is appriciated.