Hi everyone, I want to design 0-10V transmitter for load cell but ı can't choice any op-amp. Please helping me for this. Thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi user4864313,
That really isn't enough information for us to be able to assist you. Does the transmitter drive the load cell, or does it drive a line following the load cell? Take a look at the questions above in the " When posting, please include the following:" section and provide as much information as you can.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hello user4864313,
I am not sure of your load cell configuration, but they are often a resistive bridge where one or more of the resistors in the bridge change value in response to the application of the external weight. Most often the bridge has a differential output voltage that is zero when no weight is applied, and it increases as the weight increases. The differential output voltage is ideally followed by a differential amplifier made up of a pair of op amps, or an integrated instrumentation amplifier. An example of a bridge amplifier is seen below that uses OPA2277 dual op amp. Some instrumentation amplifiers that may be used for this task are listed within the schematic.
If you need a 4 to 20 mA current output the load cell amplifier can be followed by a Precision Voltage-to-Current Converter/Transmitter such as the XTR111. Additionally, there is the PGA300 which is a complete pressure sensor solution offering 4 to 20 mA output current capability. You can view the datasheet here:
Regards, Thomas
Precision Amplifiers Applications Engineering
Thanks for reply, Thomas Kuehl. My Loadcell is some like your schematic and resistance is 100 ohm. I use OPA177 but when no weigh on load cell ı can't see 0 V to output. Maybe OPA2277 help to me. I will try and tell you.
Hello user4864313,
The input offset voltage of any op amp will be amplified by the gain used in the circuit. Since the offset voltage is seldom 0 V, but some real amount possibly as high as the maximum value, the output will not be 0 V with zero weight. The OPA2777 input offset voltage is rated to be a little lower than that of the OPA177, but you still will likely see a non-zero output with no load on the cell.
Both the OPA177 and OPA277 single op amps have offset control pins which can be used to zero the output offset when the cell is unloaded. The feature is not available on the OPA2277 dual op amp.
Regards, Thomas
Precision Amplifiers Applications Engineering
Thanks for reply,
I try to use OP177, but ı have not see 0 V output when ı use a trim trimpot. Also ı search internet and ı see trimpots break down during use. Now ı want to design a digital 0-10 V transmitter and when ı search an internet ı see ad5721 and ad5761 DAC but ı could not found like this DAC in TI. Do you have a DAC that I can recommend
user4864313,
TI does not have exact replacements for the two DACs you mention, but there are others that TI offers that should work.
I am not involved with the DAC products, but looking over you requirements the DAC8871 may be provide good solution. It offers 16-bit resolution and an output voltage up to +/-18 V, which is set by the applied reference levels. It has an SPI interface. You can view the datasheet here:
If you have questions about applying a DAC in this kind of application the Data Converter E2E forum may be able to best assist you.
Regards, Thomas
Precision Amplifiers Applications Engineering