Part Number: THS7373
Hello,
I have some questins with THS7373 design need your help.
1.Can i use two 150 ohm pull down resister in RGB signal torouting RGB trace impedance with 37.5 ohm and 50 ohm?
2.Page 38 (Cout =330uF) and Page 42 ( Cout = 470uF) of THS7373 datasheet, the Cout pin + direction is difference, which one is right?
3.Page 42 of THS7373 datasheet demo circuit has use two capacitors ( 470uF and 0.1uF), do they need to implement at the same time?
Does 470uF design for low frequency bandwidth and 01uF for high frequency bandwidth?
4.Can i use 0,1uF MLCC as Cout for 1920x1200 resolution?
5.Does Cout is necessary? why i need to use it?
Thanks
Regards
C. A. Lai