Hello sir, i have LMV358 Breakout board( Red MOdule - 100 times gain). I used it to amplify my input signal 100 mv square wave. but my output generated by LMV358 is like attached file. i did not get an actual square wave as an output why? suggest me
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello sir, i have LMV358 Breakout board( Red MOdule - 100 times gain). I used it to amplify my input signal 100 mv square wave. but my output generated by LMV358 is like attached file. i did not get an actual square wave as an output why? suggest me
Part Number: LMV358
hello sir, can i use LMV358 red module for 10 HZ frequency??
how much input i can give to the module in terms of mili volt?
if my input is 100 mv then how much output generated?
Mehul,
Let's see 100mV * 100 = 10V; you have a 5V supply so 10V is not possible.
Is input always a square wave? Is desired output always 0V to 5V square wave?
yes my input is always square wave. one more thing sir when i set high frequency then it's good output.
can this module use for low frequency like 10 HZ? I want to amplify 10 mv square wave
Mehul,
I believe you have a bad connection in your circuit. LMV358 does work well at 10 Hz.
Here are two different ways to get a full scale output.
The top amp has a gain of 100. However, the VIO error of the device (up to +/-7mV) also get 100 Gain. So VF1 = (VIN + VIO) * 100
The bottom amp is an inverting comparator with one input at 50mV. So VF2 = 0V if VIN >50mV or 5V if VIN <50mV. The output can be noninverting if the input pins are swapped.
it has only 4 connections.
Thanks for your reply sir,
but please provide full rating of 16 micro Faraday capacitor? how much volt capacitor i need to buy?
in my module value of t these high pass capacitors are? do i need any precautions before removing these capacitors with solder iron?