Part Number: OPA2192
Other Parts Discussed in Thread: OPA2140
The data sheet states only the typical value for GBW, 10MHz along the whole voltage range.
I have determined through simulations that the design is fairly sensitive to variations in this parameter. Knowing the minimum value will help me to determine if the calibration range of the circuit is OK. Moreover, calibration is sensitive to GBW variation so it would help knowing how much it varies with temperature, for a delta T of 30°C, from 10 to 40°C ambient temperature.
Regarding Slew Rate, I need to know the minimum to make sure I have enough margin to guarantee the design will work with the input signal I drive it with.
FWIW currently we are using the OPA2140 in a similar design. It works OK but the circuit requires some warm-up time before it is available. The OPA2140 replaced another part from AD that had a higher variability and caused calibration issues. The replacement apparently fixed the calibration issue but I would like to avoid the warm-up in this new design if I can. I need to reduce the supply voltage to reduce power consumption. Using OPA2192 will allow me to reduce it further as it is RRIO.