Part Number: INA213
Other Parts Discussed in Thread: INA282, INA210, INA193, INA271-HT, INA200, INA270, INA240, INA203, LM5056A, INA206
Hello,
Looking for a bit of help with a re-design where the original engineer is no longer here. We currently use an INA213A and it has suffered from the latch up issue described in the datasheet, even though we are at approximately 1KV/µs. Historically we tried the recommended ferrite and cap approach and this did not work so we have ended up with an RC filter to stop these fast transients.
Now we are re-designing this PCB we are considering the INA213B as a replacement to allow us to remove the RC filter (which is desirable as we manually select capacitors to remain in tolerance). Can you confirm that this has completely fixed the issue and what the transient robustness is of the INA213B (what is the maximum dV/dt we can apply)?
I have also seen the INA282 which may be suitable but seems to have a much larger gain error, but I think this may be because it is stated over a larger voltage variation, however I am unsure. If this is the case are there comparable numbers?
Finally are there any others that I could consider?