This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1301: Does there have a mathematical formula about AMC1301's out votage and IN votage

Part Number: AMC1301

Dears 

there only one form describe the relationship of output voltage input voltage. So does there have one mathematical formula about the relationship about the output voltage input voltage?

  • Hi Keiven, the nominal gain of AMC1301 is 8.2, so you only need to multiply 8.2 and differential input voltage to get the differential output voltage. For example, the input differential voltage is 50mV, so the differential output voltage will be 410mV, and the result is similar with the form you mentioned before.