Other Parts Discussed in Thread: OPA196
Hi,
My customer meet one issue when I used TL072.
First, when they configure it as amplifier, it works normally. the input current is about 6mA.
When they configure TL072 as a comparator, the input current increase a lot and total pow loss increase to 0.68W, the IC is hot. But when they choose the JL412BPA , it works normally with same applications.
My questions is:
1. TL072 could be configured as comparator, right?
2. Any considering when configure as comparator?
3. What's the potential root casue?
Vincent Zhang