Other Parts Discussed in Thread: LMV321A
Hi guys I need to come up with a complete list of TI low voltage op amps (0V to 2.7V maybe 3V) that have phase reversal protection or prevention circuitry built in. It is a parameter I can't search on. I'm only interested in op amps that come in single package. I only want max 6 pins. I need SC70 package or smaller. Kind Regards Paul.