Part Number: INA122
Other Parts Discussed in Thread: LOG114, OPA388, TINA-TI
I am looking for a solution to measure the wide current range from 1uA to 300mA on a 3V rail. If it not possible to do for such high range and precision, we can further split this in two and use two amplifiers 1uA - 100uA & 1mA to 300mA. I tried and refer other but bias current and the differential voltage at the port (V drop not expected more than 0.05V on 3V rail) was the area I doubt. Please suggest. The output voltage after amplifier will be input to 3.3V ADC to read the current value.