Hi team,
As customer want to know the max power dissipation of THS6301RSAR when it works, and I see dynamic power consumption and quiescent current in the datasheet. To get the max power dissipation, whether we need to add this two? for example, when THS6301 is working at the drive mode 1, the total power dissipation would be P=220mW+15.9mA*12, is it right?
Best Regards
Zhengquan Lu