Part Number: AMC1311
Other Parts Discussed in Thread: XTR111,
Hello
I am Designing an Isolated 0-20 mA corresponding to a 0-2V Isolated signal .
I am planning to use AMC1311 Isolator in conjunction with XTR111 ( and an External P Ch MOSFET NTP2955 )
to generate a 20 mA O/P proportional to 0-2V Input to AMC1311 .
Can I use the OUTP & OUTN with a 2 uS Filter to directly connect to Vin & Set of XTR111 ;
or do I need an additional Op Amp in between as a Diff Amp .
Basic proposed Ckt is as follows :