Part Number: OPA4330
Dear all:
When I use OPA4330 operational amplifier, waveform bias occurs when I add sine signal abruptly. The following are circuit diagram and waveform diagram
Please look it up and give me some advice?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you please explain the sentence
"waveform bias occurs when I add sine signal abruptly"
The input signal is an analog sinusoidal wave with a frequency of 50Hz and an adjustable amplitude. The input signal goes IN from IN+ and the reference is 2.5v.When I pass in the input signal (the input signal mutates), the output signal will drift for the first few cycles.Why?
Hi Kai:
The input signal is an analog sinusoidal wave with a frequency of 50Hz and an adjustable amplitude. The input signal goes IN from IN+ and the reference is 2.5v.When I pass in the input signal (the input signal mutates), the output signal will drift for the first few cycles.Why?