Other Parts Discussed in Thread: TINA-TI
Hi,
I am looking for Voltage-to-Current Converter Evaluation Kit for one of my test bench setup, accuracy is not that important. Output current of range 0 to 25mA and max input voltage available is 12V so a varying voltage of 0 to 5V or 0-10V can be made available. I am in need of two channel circuit and as it is test bench setup i am expecting a cheaper option/solution.