Part Number: THS4151
Other Parts Discussed in Thread: AMC1300, , THS4131
Dear sir,
We are using AMC1300 for current measurement.
Measurement range : 0 to 40Arms
Shunt resistance : 2mOhm
High side voltage input : 113.12mV peak
low side voltage output : 927.584mV peak
measurement signal frequency : DC-20kHz
We need to connect this signal to analog input module having the input signal range of +/-10V. So we wish to have the gain of 10. (input signal :927mV and output signal : 9.27V). we selected THS4151 amplifier.
Please find the below circuit and kindly verify the same to proceed with implementation. (As an alternative, could you please suggest any amplifier supports for the dual power supply and output signal in the range of +/-10V).
Thanks & regards,
Rajasekaran.