This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TLV9302: What are the best cross reference replacement for the MC33202, MC33172, and MC33178 devices? P2P is preferred.

Part Number: TLV9302
Other Parts Discussed in Thread: TLV9102, TLV9352, , TLV9152

Hello,

I need to identify replacement op amps for the MC33202, MC33172, and MC33178 devices. What are the best P2P(Pin to Pin) replacement amplifiers from TI?

Thanks!

  • Hi Katherine,

    Consider the TLV9102 or TLV9152 for 16V designs, or if higher voltage is required consider the TLV9302 or TLV9352 for up to a 40V power supply range.

    Here is a side by side comparison of the 4 recommended devices.

    Here is a table showing the performance differences between MC33202, MC33172, MC33178, and the recommend devices.

    ► Part Number
    MC33202
    TLV9102
    TLV9152
    Manufacturer
    ON
    TI
    TI
    Num Channels
    2
    2
    2
    Vs min (V)
    1.8
    2.7
    2.7
    Vs max (V)
    12
    16
    16
    GBW (MHz)
    2.2
    1.1
    4.5
    Slew Rate (V/us)
    1
    4.5
    21
    Vos max @ 25C (mV)
    6
    1.5
    0.665
    Drift typ (uV/C)
    2
    0.6
    0.35
    Rail-to-Rail
    In, Out
    In, Out
    In, Out
    Iq typ (mA)
    0.9
    0.12
    0.56
    Vn (nV/rtHz)
    20
    30
    9.5
    Isc typ (mA)
    80
    80
    80
    Ibias typ (pA)
    80000
    10
    10
    Operating Temp (°C)
    -40 to 85
    -40 to 125
    -40 to 125

    ► Part Number
    MC33172
    MC33178
    TLV9302
    TLV9352
    Manufacturer
    ON
    ON
    TI
    TI
    Num Channels
    2
    2
    2
    2
    Vs min (V)
    3
    4
    4.5
    4.5
    Vs max (V)
    44
    36
    40
    40
    GBW (MHz)
    1.8
    5
    1
    3.5
    Slew Rate (V/us)
    2.1
    2
    3.5
    20
    Vos max @ 25C (mV)
    4.5
    3
    2.5
    1.8
    Drift typ (uV/C)
    10
    2
    2
    1.5
    Rail-to-Rail
    In to V-
    No
    In to V-, Out
    In to V-, Out
    Iq typ (mA)
    0.44
    0.9
    0.15
    0.8
    Vn (nV/rtHz)
    32
    7.5
    33
    15
    Isc typ (mA)
    5
    80
    60
    60
    Ibias typ (pA)
    20000
    100000
    10
    10
    Operating Temp (°C)
    -40 to 85,
    -40 to 125
    -40 to 85
    -40 to 125
    -40 to 125

    Thank you,

    Tim Claycomb