Other Parts Discussed in Thread: TL052
Hello,
VCC+ and VCC- can be powered up in any order?
Or they must power up the same time?
Best regards,
K.Hirano
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kazuhiko,
It is highly recommenced that both VCC+ and VCC- are powered up at the same time or very close to each other. The reason is because the op amp internal circuits are not designed to have one supply turned on before the other. Also make sure during this power up no signal is applied at the input pins.
Regards,
Bala Ravi
Hi Kazuhiko,
we use many thousands of the TL052 in our products and never had any problems with unequal power-ups and power-downs. Having said this, as already mentioned by Bala, it's really important that you never violate the absolute maximum ratings, not even briefly! Also, the power supply must be latch-up protected. I have discussed this issue in the following posts:
Kai