Other Parts Discussed in Thread: , , LMV358
Hello,
I'm using LM2904 to make a differential amplifier circuit to measure the high DC voltage(200Vdc~300Vdc). The circuit is shown as below:
This circuit works well, but when a common voltage is added to the differential input(eg. ~40V), the output of LM2904 will go higher(>500mV). 3pcs of PCB have the same test results.
But if the LM2904 on board(soldered by production factory) is changed to LM2904B(which is the sample from TI), the common voltage added to the input will NOT influence the output of LM2904B.
Does that mean the LM2904 on board was broken during production? or which parameter of LM2904B is better than LM2904? thanks!