Part Number: INA317
Other Parts Discussed in Thread: LM7705, TINA-TI
Hi,
I am applying a 100Hz, 10mV pp, sine wave from a function generator to test the below circuit. I have made following changes to my circuit: gain to ~101,Rg =1kOhm,removed C7, D3,D4 from my original circuit. In the beginning, my output, is as per my initial gain calculations(~600mV) but slowly the output ramps up constantly and eventfully the output saturates closer to supply 3. 3V DC. Removing D3, D4 slowed down the ramping of the output a little bit. Additionally, I am wondering why my output signal is a constant dc instead of a sine wave, my input frequency of 100 Hz is within limits specified in section 6.5 of the datasheet.
Thanks,
Jagbir