Other Parts Discussed in Thread: INA219
Hi,
I am working with the INA219 and I am getting incorrect shunt voltage readings. They appear to be double what I would expect given my current load and what I measure across the resistor with a voltmeter.
My test setup is as such: 2m Ohm shunt resistor, 100mA load, bus voltage of 11.5. This is similar to the example setup used in the datasheet, so I initially used those same configuration parameters - Configure: 019Fh, Calibrate: 5000h. I have since changed the configure register to 1FFFh, which is 16V Range, 8 PGA, and 128 sample averaging, hoping to get more precision. I get the same results.
The INA219 reads shunt voltage of 0.4mV, bus voltage of 11.484V, and reads the current at 225mA, whereas with my multimeter I am getting 0.2mV, 11.48V, and 100mA. What could be causing this problem?
Thanks!
Justin