Other Parts Discussed in Thread: INA110, INA217, INA128
I have a circuit that I originally put together a couple of years ago and it seemed to work quite well. It is an amplifier for a low impedance sensing element (around 25 ohm) that puts out a very small dc voltage. The current batch seems to exhibit a fairly large start-up offset that slowly changes and eventually stabilizes. This takes several minutes.
For testing purposes I disconnected the 217 from the second stage and removed the sensing element, shorting the inputs together. The amp is powered by +/- 12V, has a 220 ohm gain resistor for a gain of about 46, and has a 10k resistor from each input to ground. The reference pin is grounded.
On power up the output will show about a 8-10 mV reading that decreases to around 4 mV after 10 minutes. Is there something I can change to reduce this? Was I just lucky that the first batches didn't do this?
Confused,
Jerry