I have an application where I am reading a voltage across a shunt resistor. Currently, I am able to take good voltage readings when supplying DC power through the shunt but when I try using an AC power supply, I get skewed data. I believe putting an isolation amplifier will solve the problem. The set up is a variac (connected to 208V building power) supplying power to a resistance heater and I am using a shunt resistor to calculate the current so I can then find the power of the heater. I am hoping to get about 5 kW of power from the resistance heater with a resistance of ~10 ohms. Additionally, the shunt being used is .001 Ohms. I would need a gain of 1, I'm just trying to isolate from the common mode of the variac. Would any of the isolation amplifiers sold by TI work for this particular application? Any additional information would be much appreciated.