Other Parts Discussed in Thread: AFE031
Hi,
I d like to build a power line communication card.i was exploring AFE031.
I have a analog communication interface that employs a 4 wire analog communication interface that transmits/receivies Plain Tones via telephone lines.
I d like such that the same analog interface card should be able to select whether to use the telephone wires or Power Lines for communication as the transmission media.
In such a case what will be the simplest solution to achieve the same?
So say
1.if im using telephone wires i will be using 4 wire standard interface.
2.if im using power line communication interface then
Can the same 4wire/2wire interface can be used to communicate to another Power line Card (say for eg employing AFE031).I ve seen a two wire interface in the same..Can i use it?
or shall i use the decoded signals in the digital domain in the analog card and shall employ some digital communication standard to communicate with the AFE031 in the power line communication card?
Thanks for any help
Regards
Stephen